i.MX 8M Mini - GPIO current capability

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX 8M Mini - GPIO current capability

2,307 Views
RobotDR84
Contributor I

I need to know how much current the GPIO can source and sink.

 

For example, pins P108 and P109 (GPIO_0, GPIO_1).

 

The datasheet says the output voltage of the pins was tested at 9.6 mA and held 1.8V (section 3.5, table 21).

But then I see the data sheet says the PVCCx1P8 says 3mA max but I'm not sure what "GPIO pre driver" means.

 

Thank you for your help.

0 Kudos
Reply
2 Replies

2,300 Views
RobotDR84
Contributor I

Thank you for your response, but I am still a bit unsure of what you're saying.

0 Kudos
Reply

2,302 Views
KalaimaniArumugamdev
Contributor III

Hi, 

    First think, all the pin are categorised into GPIO label(From table 7) and digital I/O are categorised into GPIO pre-driver (PVCC). It's operations range from 1.65 to 1.95 volts 3mA. But table no21 mentioned,  all the peripheral which is classified in table 7 

0 Kudos
Reply