Hi,
In section 2.1.2 (A-53) and Section 2.1.3 (M-4) of the "i.MX 8M Mini Applications Processor Reference Manual" documents the chip memory map. I have a couple of questions:
1) Can you confirm the address range 0x40000000-0xbfffffff on both the A-53 and M-4 refer to the identical DDR memory cells (i.e. writing 1 to 0x40000000 or 0x0000000040000000, will result in both the A-53 cores and the M-4 core reading a 1 from 0x40000000 or 0x0000000040000000) and that DDR can be viewed as share memory mapped to identical memory?
2) In Section 2.1.3 page 24, the address range 0x10000000 - 0x1ffdffff is allocated to "DDR Code alias". Where in the DDR address range of 0x40000000-0xbfffffff is this alias mapped (i.e if I write a 1 to 0x10000000 where in the DDR address range to this 1 appear)?
Thank you.
Solved! Go to Solution.
Hi Said
1. yes confirmed.
2. "DDR Code alias" is mapped to beginning of DDR address range,
writing a 1 to 0x 0x10000000, 1 will appear on 0x40000000.
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi Said
1. yes confirmed.
2. "DDR Code alias" is mapped to beginning of DDR address range,
writing a 1 to 0x 0x10000000, 1 will appear on 0x40000000.
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Igor, thanks a lot for your quick and helpful feedback!
Cheers,
Said