i.MX 8 M Plus Current Source and Sink

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

i.MX 8 M Plus Current Source and Sink

572 次查看
Will_Robertson
Contributor III

Hi,

I'm very sorry to ask such a basic question.

Roughly how much current can be sourced or sinked directly by pins configured as output pins on the i.MX 8 M Plus using 3.3 V logic?

I was able to find the different output strengths that could be set in the reference manual but I haven't been able to find how much current can safely be sourced or sinked to these pins.

Will

0 项奖励
回复
4 回复数

553 次查看
Chavira
NXP TechSupport
NXP TechSupport

HI @Will_Robertson!

Thank you for contacting NXP Support!

 

That information can be consulted in the datasheet.

 

Best Regards!

Chavira

 

0 项奖励
回复

551 次查看
Will_Robertson
Contributor III

Hi @Chavira 

I read the data sheet before asking and couldn't find this information in the data sheet. It may be in the reference document which is 7428 pages long but I haven't been able to read all 7428 pages.

Will

0 项奖励
回复

542 次查看
Chavira
NXP TechSupport
NXP TechSupport

HI @Will_Robertson!

 

We mention that values but not in a table.

 

We provide a formula to calculate but the typical values for iMX8MP are the next:

 

DSE_X1:  120 Ω
DSE_X2: 60 Ω
DSE_X4:  30 Ω
DSE_X6: 20 Ω

 

With the impedance values you can calculate the maximum current if you are using 3.3v or 1.8v

 

Best Regards!

Chavira

0 项奖励
回复

533 次查看
Will_Robertson
Contributor III

Hi @Chavira 

Thank you very much. The ability to set the output impedance is very valuable and innovative functionality in the i. MX 8M Plus and gives it a significant advantage over other SoCs where an additional chip would be needed to achieve this.

This will significantly ease electronic design and reduce chip count in many systems as well as giving much better fault tolerance leading to better long term robustness and reliability

Will

0 项奖励
回复