i.MX 7ULP Alternative RTOS Support

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

i.MX 7ULP Alternative RTOS Support

1,481件の閲覧回数
dto10000
Contributor I

Hi,

I saw that the i.MX 7ULP M4 processor supported FreeRTOS and MQ RTOS. The device that I'm working on is planning on using ChibiOS, and I was wondering if it were possible to run alternative RTOS's on this core.

Would it be possible to port over the RTOS code over to ChibiOS, or is there another method that I could use to run that OS on the core?

Thanks!

0 件の賞賛
返信
2 返答(返信)

1,466件の閲覧回数
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello dto10000,

 

NXP offers FreeRtos and MQXRtos but MX7ULP is able to run chibiOS, you can find more in the ChibiOS web page.

https://www.chibios.org/dokuwiki/doku.php

 

Regards

0 件の賞賛
返信

1,463件の閲覧回数
dto10000
Contributor I

ah I see, you can't run another OS on the mx4 core. Thanks!

0 件の賞賛
返信