Hi team,
Could you provide the report of 1G Ethernet Throughput Performance of i.mx 7?
The processor is MCIMX7D7DVM10SD.
Thanks.
Hi @joanxie ,
Is it possible to have the result of RX/TX bidirection throughput?
I didn't find such report intnernally
this is performance for imx6sx, but imx7d can refer to this too
"Ethernet benchmark figures, CPU at 1GHz, TX:870Mbps, RX:930Mbps"
Thanks for the prompt reply.
Is the result that test both the Ethernet TX and RX throughput in the same time?
should test RX and TX separately, I don't find RX/TX bidirection result