i.MX 6UL USB support CDC+HID

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX 6UL USB support CDC+HID

1,287 Views
AlvinLin1933
Contributor I

We need OTG support CDC+HID at the same time, when the device plug in PC, would you have the guideline or the demo support ?

Labels (1)
0 Kudos
Reply
3 Replies

1,269 Views
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello,

There are two USB port on i.mx6ul evk board, one is USB OTG with microUSB connector, the other is USB Host.  For HID device, customer can connect it to USB host; for Mass storage, customer can use a USB OTG to HOST cable to connect microUSB connector, and the other side of the cable is used to connect mass storage, such as moble disk or U disk.

 

Regards

0 Kudos
Reply

1,250 Views
AlvinLin1933
Contributor I

Hi Bio :

    Thank you for your reply.

    The application just use the USB OTG, so we would like to support CDC+HID at the same time, It should be realizable. I saw RT1064 have the similar demo. Please refer the attached.

0 Kudos
Reply

1,239 Views
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello,

Yes it is possible, but unfortunately its not implemented on MX6UL, you can do it in the exact way s the MXRT.

Regards

0 Kudos
Reply