i.MX 6DQ Synchronous Display Interface setup/hold Timing?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

i.MX 6DQ Synchronous Display Interface setup/hold Timing?

3,148件の閲覧回数
t-iishii
Contributor II

Hello Artur,

In thred https://community.nxp.com/thread/382105 and https://community.nxp.com/thread/446848,

We discuss about data setup and hold timing parameter about Synchronous Display Interface.

To understand IP18(Data setup time) and IP19(Data holdup time) parameter in Table 70 of datasheet(IMX6DQAEC),

It will confusion because it has two parameter both rise and fall edge in one table.

The other hands, to design a timing for LCD, only one edge need to attention.

So, attached documents that I create a separate tables for each edge.

How do you think my understanding about this parameters?

Best regards,

Ishii.

ラベル(3)
0 件の賞賛
返信
3 返答(返信)

3,014件の閲覧回数
art
NXP Employee
NXP Employee

Actually, both IP18 and IP19 parameters are referenced to the same clock edge (either rising or falling depending on the clock polarity settings), so, everything looks good on your diagram.


Have a great day,
Artur

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

3,014件の閲覧回数
t-iishii
Contributor II

Hello, Artur

Thank you for your quick response.

I will ask my customer that.

Best regards,

Ishii.

0 件の賞賛
返信

3,014件の閲覧回数
t-iishii
Contributor II

Hello

I modify attached timing document based on the datasheet timing Figure 71.

Please review a document and give me a comment for that.

Best regards,

Ishii

0 件の賞賛
返信