i.MX 6DQ Synchronous Display Interface Timing Characteristics

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

i.MX 6DQ Synchronous Display Interface Timing Characteristics

16,730 次查看
sugiyamatoshihi
Contributor V

Hi,@Artur Petukhov 従業員 

I have aquestion about Synchronous Display Interface Timing Characteristics in i.MX 6DQ data sheet.

There is a specification of data holdup/setup  timing in figure 71 and Table 70.

I think this LCD interface only output clock, data and controll signal to LCD. So, I wonder why there is setup time specification. I suppose usually data delay time and hold time from clock edge are specified for output  signal. 

I attched a doc.

I checked below, but I couldn't understand clearly.

https://community.nxp.com/message/597894

Best Regards,

Sugiyama

标签 (2)
0 项奖励
回复
14 回复数

16,376 次查看
t-iishii
Contributor II

Hi,

Artur

Possibly does "Tdsu" mean a time from local start point to data valid?

"               _______         ___|___         _______         ___"

"IPP_DISP_CLK_N|       |_______|   |   |_______|       |_______|   "

"                            Tdicu |<->|"  

"          ________________________|   |_______________ ___________"

" Tdsu(Typ)________________________XXXXX_______________X___________"

"                       Tdicd-1.24 |<-------->||<- 1.24"

"          ________________________|          |_______________ ____"

" Tdsu(min)_________________________XXXXXXXXXXX_______________X____"

"                                  | <-- local start point"

Normally, data setup mean from data valid to edge for data latch.

"             ___________                   __________"

" data enable            |_________________|"

"  Tdsu                           |<------>|" 

"             ____________        |________|__ _______"

"  DATA       ____________XXXXXXXX____________X_______"

Best regards,

Ishii.

0 项奖励
回复

16,376 次查看
t-iishii
Contributor II

Hello Artur

Thank you for your comment and sorry for my late reply.

If DISP_CLK_UP = 0x00 and DISP_CLK_DOWN=0x02, 

IP18 Tdsu(Min) will larger than Tdus(Typ) value.

We use following register setting

   DI_CLK = 108MHz

   DISP_CLK_PERIOD = 0x20

   DI_CLK _PERIOD     = 0x10

   DISP_CLK_UP           = 0x00

   DISP_CLK_DOWN    = 0x02

in this time

Tdiclk = 9.26nsec

Tdicd = 1/2(9.26ns * ceil( 2x (0x02/2) / (0x10/16) ) =  9.26

Tdicu = 1/2(9.26ns * ceil( 2x (0x00/2) / (0x10/16) ) = 0

Tdus(Min) = Tdicd - 1.24 = 9.26 - 1.24 = 8.02

Tdsu(Typ) = Tdicu = 0

So Tdus(Min): 8.02 > Tdsu(Typ): 0

In this case,  how do we think about it?

Best regards,

Ishii.

0 项奖励
回复

16,376 次查看
karina_valencia
NXP Apps Support
NXP Apps Support

art‌ please continue with the follow up

0 项奖励
回复

16,376 次查看
art
NXP Employee
NXP Employee

Actually, there are just some confusing names for the timing parameters. And, you are right, here IP19 can be treated as the Data Delay time and IP18 - as the Data Hold time parameters.


Have a great day,
Artur

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

16,376 次查看
sugiyamatoshihi
Contributor V

Hi, Artur,

Thank you for clarifing it.

Thanks,

Sugiyama

0 项奖励
回复

16,376 次查看
sugiyamatoshihi
Contributor V

Hi, Artur,

I wrote a document to understand easier to to understand the DI clock timing.

Could you review the doc. if my understanding is correct?

Best Regards,

Sugiyama

0 项奖励
回复

16,376 次查看
art
NXP Employee
NXP Employee

Yes, your understanding is correct.

Best Regards,

Artur

16,376 次查看
t-iishii
Contributor II

Hello Artur,

I'm very confuse about IPP_DISP_CLK porarity in Figure 71 in IMX6DQAEC.

Mr Sugiyama say in attached document, that Figure 71 is missed,

Between local start point and falling edge of IPP_DISP_CLK is Tdicd.

Between local start point and rising edge of IPP_DISP_CLK is Tdicu.

But you say A.2(Answer of Q2) in thread About setup/hold time of synchronous display in i.MX6DQ. 

to Figure 71 is correct.

Which is a correct answer?

If it is not clear, we can not discuss about table 70 in IMX6DQAEC,

because it is very ambiguous about IP18, IP19 meening.

My goal is to understand how to define each register value to fit a requirement of each LCD panel.

For it, please express a meaning of each timing parameter like,

   IP18 : time from IPP_DATA valid to falling edge of IPP_DISP_CLK if IPP_DISP_CLK is not inverted..

   IP19: time from falling edge of IPP_DISP_CLK, if IPP_DISP_CLK is not inverted.

      Note: DISP_CLK_DOWN > DISP_CLK_UP.

Best regards,

Ishii.

0 项奖励
回复

16,376 次查看
art
NXP Employee
NXP Employee

Dear Takayuki Ishii,

Yes, you are right. In case of IPP_DISP_CLK is not inverted, these timings can be treated as follows.

IP18: IPP_DATA valid to falling edge of IPP_DISP_CLK.

IP19: falling edge of IPP_DISP_CLK to IPP_DATA invalid.

Best Regards,
Artur

0 项奖励
回复

16,376 次查看
t-iishii
Contributor II

Hi,

Artur

Thank you for your response.

Which timing does it triggered a data transition?

Local start time is correct?

Best regards,

Ishii.

0 项奖励
回复

16,376 次查看
art
NXP Employee
NXP Employee

Yes, you are right. The local start point triggers the data transfer according to the timings above.

Best Regards,

Artur

0 项奖励
回复

16,376 次查看
t-iishii
Contributor II

Hi Artur, 

Thank you for your kindly support.

But I can not explain this logic to my customer yet.

Following are register value  by Linux BSP 4.1.15 + i.MX6QSabre-SDP

  • IPU2_PM :0x02A000E0 = 0x08100810 -> 0b00-00 1000 0-001 0000 : 00-00 1000 0-001 0000
    ** DI1_CLK_PERIOD_1[29:23] = 0b0010000 = 0x10
    ** DI1_CLK_PERIOD_0[22:16] = 0b0010000 = 0x10
    ** DI0_CLK_PERIOD_1[13:7] = 0b0010000 = 0x10
    ** DI0_CLK_PERIOD_0[6:0] = 0b0010000 = 0x10
  • IPU2_DI0_BS_CLKGEN0:0x02A40004 = 0
    ** DI0_DISP_CLK_OFFSET[24:16]
    ** DI0_DISP_CLK_PERIOD[11:0]
  • IPU2_DI0_BS_CLKGEN1:0x02A40008 = 0
    ** DISP_CLK_DOWN[24:16]
    ** DISP_CLK_UP[8:0]
  • IPU2_DI1_BS_CLKGEN0:0x02A48004 = 0x00000010
    ** DI1_DISP_CLK_OFFSET[24:16] = 0000
    ** DI1_DISP_CLK_PERIOD[11:0] = 0010
  • IPU2_DI1_BS_CLKGEN1:0x02A48008 = 0x00010000
    ** DISP_CLK_DOWN[24:16] = 01
    ** DISP_CLK_UP[8:0] = 00

Please inform me, how design IPU timing to fit LCD panel specification.

Best regards,

Ishii.

0 项奖励
回复

16,376 次查看
t-iishii
Contributor II

Hi

Can anyone comment to me?

Best regard,

Ishii.

0 项奖励
回复

16,376 次查看
sugiyamatoshihi
Contributor V

Hi, Artur,

Thanks for  review and answer.

Best Regards,

Sugiyama

0 项奖励
回复