Dear NXP,
I know that "hwcomposer_viv.imx6.so" is for hardware compositor (GC320) library in android.
Which API should I use in Linux:
according to "L3.0.35_4.1.0_docs"?
Yours,
Hi Ali
1. seems this is gpu driver, description can be found in
Graphics Processing Unit (GPU) Chapter of Linux Manual included in L3.0.35 documentation
2. proprietary gpu libs are provided as binaries only, one can try to get
sources using local marketing office.
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------