hwcomposer_viv.imx6 library in android

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

hwcomposer_viv.imx6 library in android

1,123件の閲覧回数
ali_sarlak
Contributor III

Dear NXP,

I know that "hwcomposer_viv.imx6.so" is for hardware compositor (GC320) library in android.

  • What's the equivalent library that do the same job in Linux (L3.0.35)?

Which API should I use in Linux:

  • i.MX_6_2D_API
  • i.MX_6_G2D_API
  • i.MX_6_Series_Wayland_Weston_User_Guide
  • Directfb1.4

according to "L3.0.35_4.1.0_docs"?

Yours,

0 件の賞賛
返信
1 返信

948件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Ali

1. seems this is gpu driver, description can be found in

Graphics Processing Unit (GPU) Chapter of Linux Manual included in L3.0.35 documentation

http://www.nxp.com/webapp/Download?colCode=L3.0.35_4.1.0_LINUX_DOCS&Parent_nodeId=133769948107170617... 

2. proprietary gpu libs are provided as binaries only, one can try to get

sources using local marketing office.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信