how to use mfg tools

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

how to use mfg tools

1,797件の閲覧回数
chewhouming
Contributor III

in DOS, in Sb_loader folder, i run

sb_loader.exe -f u-boot-mx6q-sabrelite.bin

it reply waiting for HID device for 2 seconds

I brick my sabrelite board, try using mfg tools but without successful.

i tried following link http://comments.gmane.org/gmane.linux.linaro.devel/11942

Choose Options->Configuration...->USB-Ports

  and search for something like "Linux-File-Stor..." or "HID-device..."

There is no something like "Linux-File-Stor..." or "HID-device..."

1 返信

1,642件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi chew

you can test if USB interface is healthy with SDK

(one can run tests with jtag)

i.MX 6Series Platform SDK

or probably just replace processor.

Best regards

chip

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------