Hello
When I compile the kernel, How to set the machine name for 8MMINID4-EVK?
I use below for BSP.
- repo init -u https://source.codeaurora.org/external/imx/imx-manifest -b imx-linux-rocko -m imx-4.9.88-2.0.0_ga.xml
thanks
Bryan
解決済! 解決策の投稿を見る。
hello NXP
Move to sources/meta-imx/meta-bsp/conf/machine.
there is imx8mmddr4evk.conf file.
thanks
Bryan
hello NXP
Move to sources/meta-imx/meta-bsp/conf/machine.
there is imx8mmddr4evk.conf file.
thanks
Bryan
After I set MACHINE to imx8mmddr4evk,
===
$DISTRO=fsl-imx-wayland MACHINE=imx8mmddr4evk source imx-setup-release.sh -b build-core
$bitbake core-image-base
$DISTRO=fsl-imx-wayland MACHINE=imx8mmddr4evk source imx-setup-release.sh -b build-image-core
$bitbake imx-image-core
===
Each above two case, build error happened as below.
===
ERROR: core-image-base-1.0-r0 do_image_wic: Execution of '/nvme1/bryan/iot/imx8m-mini/imx-yocto-bsp/build-core/tmp/work/imx8mmddr4evk-poky-linux/core-image-base/1.0-r0/temp/run.do_image_wic.28387' failed with exit code 1:
INFO: Creating image(s)...
ERROR: A native program mkfs.ext4 required to build the image was not found (see details above).
Please make sure wic-tools have e2fsprogs-native in its DEPENDS, build it with 'bitbake wic-tools' and try again.
WARNING: /nvme1/bryan/iot/imx8m-mini/imx-yocto-bsp/build-core/tmp/work/imx8mmddr4evk-poky-linux/core-image-base/1.0-r0/temp/run.do_image_wic.28387:1 exit 1 from 'BUILDDIR="/nvme1/bryan/iot/imx8m-mini/imx-yocto-bsp/build-core" wic create "$wks" --vars "/nvme1/bryan/iot/imx8m-mini/imx-yocto-bsp/build-core/tmp/sysroots/imx8mmddr4evk/imgdata/" -e "core-image-base" -o "$out/" --no-fstab-update'
ERROR: Logfile of failure stored in: /nvme1/bryan/iot/imx8m-mini/imx-yocto-bsp/build-core/tmp/work/imx8mmddr4evk-poky-linux/core-image-base/1.0-r0/temp/log.do_image_wic.28387
===
BUT If I set MACHINE to imx8mmevk, build error did not happended. BTW why did not generated sdcard image file ?
BR
Bryan
Hi
With emmc ,Bootloader is “imx-boot-imx8mmevk-sd.bin-flash_evk”.Rootfs and kernel is “imx-image-full-imx8mmevk-20200708060549.rootfs.bz2 ”
Open shell/terminal:
uuu -b emmc_all bootloader_name rootfs_name ----------------------EMMC
uuu -b sd_all bootloader_name rootfs_name ----------------------SD
update all images: uuu -b emmc_all imx-boot-imx8mmevk-sd.bin-flash_evk imx-image-full-imx8mmevk-20200708060549.rootfs.bz2
update bootloader: uuu -b emmc bootloader_name
More details can see uuu.pdf.
Hello
How did I found that information about imx8mmddr4evk ? I can't found that information at any pdf documents.
thanks
Bryan
Hi
It was defined in yocto and not mentioned in pdf.
BR
Zhiming
so,
How does someone at first to build for 8MMINID4-EVK know this MACHINE ?
thanks
Bryan
Could you guide for me that the location for yocto?
Hi
Host name is imx8mmddr4evk
BR
Zhiming
Hello
How did I found that information about imx8mmddr4evk ? I can't found that information at any pdf documents.
thanks
Bryan