how to flash android demo image to SD card through a CARD READER -

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

how to flash android demo image to SD card through a CARD READER -

1,361 Views
Tooght
Contributor III

Hi,

I need to flash an android demo image(currently available android-13.0.0_1.0.0_image) to an sd card. But the thing is I do not have usb connection with the board. So, I am wondering if it is possible to flash the sd card through a usb card reader instead of flashing the sd card on the dev board through usb connection with the board.

I have an i.MX 8M Quad EVK Board 

Tags (3)
0 Kudos
Reply
2 Replies

1,347 Views
Zhiming_Liu
NXP TechSupport
NXP TechSupport

You can flash Linux image by card reader but you can't flash Andoird with it. Please connect the USB port.

0 Kudos
Reply

1,339 Views
Tooght
Contributor III

Hi @Zhiming_Liu, thanks for the quick reply.

I have to do that otherwise I won't be able to use anymore the board. I have a custom board based on 8mq without mmc And booot config doesn't allows me to flash over USB. Please shed me some light how to flash by card reader.

 

0 Kudos
Reply