how to automatically start Linux

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

how to automatically start Linux

1,223件の閲覧回数
hailiu
Contributor IV

dear all,

I went through the Linux User Manual, and found that a UART port is needed to use uboot. I have not add the UART port on my board. I don't want to talk uboot, and just want to start the Linux with it. I don't suppose the UART is a must to run Linux because it is not a case for an embedded system. I just want to use the uboot to start the Linux. How to automatically start the Linux with SD card or eMMC card? 

 

thank you,

Hai

0 件の賞賛
返信
1 返信

1,217件の閲覧回数
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello Hailu,

You need connect the keyboard, and booted the board, wait for a minute a press "root" then you have linux.

 

Regards