how to application u-boot command

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

how to application u-boot command

1,464件の閲覧回数
kangmw086
Contributor III

hi

i used i.mx6 sabreauto board.

Is it possible to add / remove / modify u-boot command in application after I.MX6 board booting is completed?
I want to create a linux application that will function like 'setenv ~~', 'saveenv' in the u-boot menu when booting the board.
Do you have references or examples?

And is there a way to control it like gui instead of command in u-boot like windows cmos?
It does not have to be 'gui'. You need something to select the u-boot command.

regards!!

ラベル(2)
0 件の賞賛
返信
1 返信

1,399件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi k

as this is specific uboot question one can post it to uboot mail list

U-Boot Info Page 


Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信