Hi,
I can able to install libMSO.so.1.2 but i cant able to make symbolic libMSO.so.
DESCRIPTION = "program"
PR = "r0"
LICENSE = "GPLv2"
S = "${WORKDIR}"
LIC_FILES_CHKSUM = "file://libMSO.so.1.2;md5=49b4ca37bfccc1a103e0ea32073358e6"
SRC_URI += "file://libMSO.so.1.2"
do_install() {
install -d ${D}${libdir}/
install -m 0755 ${S}/libMSO.so.1.2 ${D}${libdir}/
ln -sf ${D}/${libdir}/libMSO.so.1.2 ${D}/${libdir}/libMSO.so
}
FILES_${PN} = "${libdir}/libMSO.so.1.2"
can any tell me to make symbolic to shared librery.
解決済! 解決策の投稿を見る。
i got the solution now i can able to install .so
FILES_${PN} += "${libdir}/*.so"
FILES_SOLIBSDEV = ""
INSANE_SKIP_${PN} += "dev-so"
we should add this three lines in .bb file
i got the solution now i can able to install .so
FILES_${PN} += "${libdir}/*.so"
FILES_SOLIBSDEV = ""
INSANE_SKIP_${PN} += "dev-so"
we should add this three lines in .bb file
Thank you so much. This seems to be the only way to do easily as of 2022-01-20.
Hi Banu,
I do not exactly understand what are you trying to do with LibMSO, i think should be LibM.so, but general information about creating symbolink links in Yocto :
TipsAndTricks/Packaging Prebuilt Libraries - Yocto Project
also to create and install a new library please check;
[yocto] How to create and install a library in yocto -- Hello Library
Hope his helps
Hi,
libMSO.so.1.2 is my application shared library. i can able to install libMSO.so.1.2 and i can't able to make symbolink to .so
do_install_append() {
install -d ${D}${libdir}/
install -m 0777 ${S}/libMSO.so.1.2 ${D}${libdir}/libMSO.so.1.2
ln -sf libMSO.so.1.2 ${D}${libdir}/libMSO.so
install -m 0777 ${S}/libMSOComm.so.1.2 ${D}${libdir}/libMSOComm.so.1.2
ln -sf libMSOComm.so.1.2 ${D}${libdir}/libMSOComm.so.1
ln -sf libMSOComm.so.1.2 ${D}${libdir}/libMSOComm.so
}
Directory of rootfs/usr/bin - there is no libMSOComm.so link.
libMSOComm.so.1 -> libMSOComm.so.1.2
libMSOComm.so.1.2
local.conf i change the priority too
# We have a conf and classes directory, add to BBPATH
BBPATH .= ":${LAYERDIR}"
# We have a packages directory, add to BBFILES
BBFILES += "${LAYERDIR}/recipes-*/*/*.bb \
${LAYERDIR}/recipes-*/*/*.bbappend"
BBFILE_COLLECTIONS += "plum"
BBFILE_PATTERN_plum := "^${LAYERDIR}/"
BBFILE_PRIORITY_plum = "6"