LAN8720A with iMX8MP

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 
2,294件の閲覧回数
khang_letruong
Senior Contributor III

Dear @igorpadykov,

I saw your support of LAN8720A Ethernet PHY for iMX8MM in following thread : https://community.nxp.com/t5/i-MX-Processors/i-MX8MM-RMII-reference-clock/m-p/952927. I would like to know if it is feasible to use that PHY with iMX8MP in recent BSPs, please ?

Thanks in advance and best regards,
Khang

 

0 件の賞賛
返信
1 解決策
2,290件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Khang

 

> if it is feasible to use that PHY with iMX8MP in recent BSPs, please

 

yes.

RMII is supported as described in sect.3.8.3 Ethernet controller (ENET)

i.MX 8M Plus Applications Processor Datasheet for Consumer Products

 

Best regards
igor

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
2,291件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Khang

 

> if it is feasible to use that PHY with iMX8MP in recent BSPs, please

 

yes.

RMII is supported as described in sect.3.8.3 Ethernet controller (ENET)

i.MX 8M Plus Applications Processor Datasheet for Consumer Products

 

Best regards
igor

0 件の賞賛
返信
2,262件の閲覧回数
khang_letruong
Senior Contributor III

Thanks @igorpadykov , I will try this!

BR,
K.

タグ(1)
0 件の賞賛
返信