how to accelerate object detection algorithm based opencv in imx6q

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

how to accelerate object detection algorithm based opencv in imx6q

1,515件の閲覧回数
hbyiwen
Contributor I

My board is imx6q, I have transplant opencv in it,and run a object detection  algorithm,but the running rate is so slow that camera can't catch anying,

1. how I can accelerate objectdetection algorithm in imx6q ?

2. I find imx6q have gpu_vivance module, can I use it accelerate objectdetection algorithm in imx6q ?

Thank you for your replay

在imx6q上跑opencv自带的目标检测(行人检测)算法程序(c++版)实在是太卡了,几乎是30秒一帧画面,想在摄像头或视频中做行人检测,不得不做加速,请教有人做过这方面的测试吗?

0 件の賞賛
返信
1 返信

1,431件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi yiwen

one can look at AN4629 Fast Image Processing with i.MX 6 Series
Fast Image Processing with i.MX 6 Series

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信