Hello,
NXP Linux USB driver has the following features :
“Peripheral mode-Supports MSC, and CDC (Communication Devices Class)
drivers which include ethernet and serial support”.
Sorry, there is not support for UVC. Customers can create own
driver, based on NXP one, using it as an example.
Have a great day,
Yuri
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------