how can we use RTIC block in iMX8QX CPU.

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

how can we use RTIC block in iMX8QX CPU.

863 次查看
deeksha
Contributor III

Please tell me, How one-time hash mode and continues hash mode is implemented in RTIC?

How RTIC works in iMX8QX CPU.

0 项奖励
回复
1 回复

822 次查看
Yuri
NXP Employee
NXP Employee

Hello,

 

  The only information regarding i.MX8X RTIC is available in the i.MX8X Security Reference Manual,

which is not publicaly available yet.

 

Have a great day,

Yuri

 

-------------------------------------------------------------------------------

Note:

- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored

 

Please open a new thread and refer to the closed one, if you have a related question at a later point in time.

0 项奖励
回复