how can i get i.mx6ull compiled in the yocto

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

how can i get i.mx6ull compiled in the yocto

2,021 次查看
hyoungkikim
Contributor IV

i want to use i.MX6ULL  and bought the i.mx6ull-evk   and installed Yocto  ( from fsl-community-bsp)

but  i coudn't  find  i.mx6ull configraution    i  just found imx6uevk configraution

and also downloaded L4.1.15_2.0.3_6ULL_patch_image but it isn't sources

could i build imx6ul-evk and use it ?

where could i get u-boot and kernel source  of L4.1.15_2.0.36ULL ?  and build in the yocto

thanks in advance

标签 (3)
2 回复数

1,723 次查看
joanxie
NXP TechSupport
NXP TechSupport

you can find all of the demo image you need for mx6ull evk from the link as below:

<MCIMX6ULL-EVK|i.MX6ULL Evaluation Kit|NXP >.

pls focus on the "Board Support Packages"

if you need to build the source code for mx6ull evk, you can refer to the document named "i.MX Yocto Project User's Guide"

and you can download the document from the link as below:

MCIMX6ULL-EVK|i.MX6ULL Evaluation Kit|NXP 

1,723 次查看
hyoungkikim
Contributor IV

thank you for  the answer

i followed the doc ....and  now in compiling ...

but if  i downloaded  the bsp from  freescale.github.io  (  2.2-codname Morty )

there is no imx6ull machine configuration    can i use imx6ul instead  ?

thank you

0 项奖励
回复