hibernation issue

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

hibernation issue

2,273件の閲覧回数
himalimunshi
Contributor I

I am trying to implement the hibernation with static image concept,able to create the hibernation image.

On first resume the boards come up properly, on subsequent boot the emmc partition gets corrupted

ラベル(2)
0 件の賞賛
返信
2 返答(返信)

1,981件の閲覧回数
b36401
NXP Employee
NXP Employee

Please note that our Linux BSP and Android BSP do not support hibernation by default.

And we have no recommendation regarding it.

Sorry for inconvenience.

I know some customers are trying to test hibernation on i.MX6 platform.   

And I heard that there are some issues with GPU. So please check this first.

Have a great day,

Victor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

1,981件の閲覧回数
himalimunshi
Contributor I

okay victor linnik

regards,

himali

0 件の賞賛
返信