gst-plugins-good add jpegenc

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

gst-plugins-good add jpegenc

2,383 Views
陈万里
Contributor I

i  compile ltib add gst-plugins-good but i cant get jpegenc 

ced0099aeb6c094c8cc37490d1c6ae83.png

and my lib have libjpeg.so 

how to get jpegenc ,thanks

Labels (1)
0 Kudos
Reply
3 Replies

2,243 Views
igorpadykov
NXP Employee
NXP Employee

Hi

ltib provides separate codecs package which includes jpegenc

please check fsl-mm-codeclib-1.7.1 on

Codecs and other Algorithms (1)

Linux Multimedia Codecs source code and deb install packages
(Gstreamer package and OpenMax packages)

i.MX51 Evaluation Kit|NXP 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

2,243 Views
陈万里
Contributor I

ok ,but my capture image is black ,whysss.jpeg

gst-launch v4l2src num-buffers=1 !  video/x-raw-yuv ! queue ! ffmpegcolorspace ! queue ! jpegenc ! filesink location="sss.jpeg"

0 Kudos
Reply

2,243 Views
Yuri
NXP Employee
NXP Employee

Hello,

  

  Looks like You are using USB camera (v4l2src).

Is Your video dev number (X) correct (/dev/videoX) ?

Is it possible to get any image from the camera ?

 

Regards,

Yuri.

0 Kudos
Reply