gps uart err

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

gps uart err

2,800 Views
zengzhaoping
Contributor II

现在我们项目gps模块使能由mcu控制,imx6在uart初始化之前就一直在收到gps数据

内核启动过程中不断打印如下log,不知道是什么原因导致的?

imx-uart 21ec000.serial: overwrite!

imx-uart 21ec000.serial: overwrite!

或

imx-uart 21ec000.serial: Rx FIFO overrun

imx-uart 21ec000.serial: Rx FIFO overrun

Labels (4)
0 Kudos
Reply
2 Replies

2,520 Views
jimmychan
NXP TechSupport
NXP TechSupport

which i.mx6 are you using? which BSP and board are you using?

is the GPS turned off when the kernel is starting? is there any GPIO to control the GPS?

0 Kudos
Reply

2,520 Views
zengzhaoping
Contributor II

我们用的是imx6d-sabresd ,bsp用的linux3.10.53+android4.4.3

gps 使能是由mcu控制;所以当内核启动的时候 gps是打开的。

0 Kudos
Reply