gpio configuration issue

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

gpio configuration issue

ソリューションへジャンプ
8,486件の閲覧回数
leeseungik
Contributor III

I test with my custom board based on sabrelite and sabreauto.

my board mainly based on sabrelite but some part are based on sabreauto.

so I want to merge some code from sabreauto to sabrelite for i2c3 usage.

first I configure pad and gpio

#define SABREAUTO_I2C3_STEER        IMX_GPIO_NR(5, 4) // from sabreauto
MX6Q_PAD_EIM_A24__GPIO_5_4, // to steer to weim and i2c3

then

1290     ret = gpio_request(SABREAUTO_I2C3_STEER, "i2c3-steer"); //SABREAUTO_I2C3_STEER

1291     printk("silee gpio request = %d \n",ret, "i2c3-steer");

gpio_request retun EINVAL

what is needed more?

gpio_request return 0 when I run sabreauto binary.

thanks.

ラベル(3)
タグ(4)
0 件の賞賛
返信
1 解決策
7,337件の閲覧回数
leeseungik
Contributor III

It’s working now the problem is I set gpio output so early before gpio chip not initialized.

I move gpio_request and output to end of board_init then It works.

Your reply is really helpful to solve it. Thanks.

BR

  Seungik Lee

元の投稿で解決策を見る

0 件の賞賛
返信
14 返答(返信)
7,337件の閲覧回数
weidong_sun
NXP TechSupport
NXP TechSupport

Hello,lee,

     Since you want to use I2C3, why you defined and iomuxed this pin as GPIO ?

Regards,

Weidong

0 件の賞賛
返信
7,337件の閲覧回数
leeseungik
Contributor III

I2C3 is desingned as same with the sabreauto reference. that's all.

and most changed parts are not work properly, I think these malfunctioning is related with gpio.

0 件の賞賛
返信
7,337件の閲覧回数
weidong_sun
NXP TechSupport
NXP TechSupport

OK, Lee,

     don't worry ! Could you share your schematic with me ? Let me see .

My Email : [email protected]

Regards,

Weidong

0 件の賞賛
返信
7,337件の閲覧回数
weidong_sun
NXP TechSupport
NXP TechSupport

Hello,lee,

     I checked your schematic, Then compared it with sabreAI board and BSP, I feel iomuxing is correct, but It seems that "mxc_iomux_v3_setup_multiple_pads()" functions was not run in "mx6_board_init(void)".

     See following code in board-mx6q_sabreauto.c:

/*If at least one NOR memory is selected we don't

  * configure IC23 PADS for rev B */

if (spinor_en) {

  BUG_ON(!spinor_pads);

  mxc_iomux_v3_setup_multiple_pads(spinor_pads, spinor_pads_cnt);

} else if (weimnor_en) {

  BUG_ON(!weimnor_pads);

mxc_iomux_v3_setup_multiple_pads(weimnor_pads,

      weimnor_pads_cnt);

} else {

  if (!board_is_mx6_reva()) {

   BUG_ON(!i2c3_pads);

   mxc_iomux_v3_setup_multiple_pads(i2c3_pads,

     i2c3_pads_cnt);

  }

}

  Please trace that above code and check if mxc_iomux_v3_setup_multiple_pads(weimnor_pads, weimnor_pads_cnt) function was run.

Weidong

0 件の賞賛
返信
7,337件の閲覧回数
leeseungik
Contributor III

code runs properly

I defined pad

342 #if __SILEE_275_I2C3__

343 static iomux_v3_cfg_t mx6q_i2c3_pads[] __initdata = {

344 MX6Q_PAD_GPIO_3__I2C3_SCL,

345 MX6Q_PAD_EIM_D18__I2C3_SDA,

346 };

347 static iomux_v3_cfg_t mx6q_extra_pads[] __initdata = {

348 MX6Q_PAD_EIM_A24__GPIO_5_4, // steering i2c3

349 };

350

351 #endif

and run folloing code in board_init function

1276 #if __SILEE_275_I2C3__

1277 iomux_v3_cfg_t *i2c3_pads = NULL;

1278 iomux_v3_cfg_t *extra_pads = NULL;

1279 int i2c3_pads_cnt;

1280 int extra_pads_cnt;

1281

1282 i2c3_pads = mx6q_i2c3_pads;

1283 i2c3_pads_cnt = ARRAY_SIZE(mx6q_i2c3_pads);

1284 extra_pads = mx6q_extra_pads;

1285 extra_pads_cnt = ARRAY_SIZE(mx6q_extra_pads);

1286 mxc_iomux_v3_setup_multiple_pads(extra_pads, extra_pads_cnt);

1287

1288 BUG_ON(!i2c3_pads);

1289 mxc_iomux_v3_setup_multiple_pads(i2c3_pads, i2c3_pads_cnt);

1290 printk("silee

0 件の賞賛
返信
7,337件の閲覧回数
weidong_sun
NXP TechSupport
NXP TechSupport

Hello,lee,

     the usage is correct , you can try to pull EIM_A24 pin up to high. Then measure voltage via R725 to check if it is high level.

weidong

0 件の賞賛
返信
7,337件の閲覧回数
leeseungik
Contributor III

with same board I tested I2C3 read/write without pullup pin with compiled as sabreauto.

I think the problem start from "gpio_request retunning EINVAL". I want to know what cause EINVAL return?

Thanks

seungik Lee

0 件の賞賛
返信
7,337件の閲覧回数
weidong_sun
NXP TechSupport
NXP TechSupport

Hello,lee,

     Do you want EIM_A24 to work as a GPIO or I2C ?

weidong

0 件の賞賛
返信
7,337件の閲覧回数
leeseungik
Contributor III

I want EIM_A24 to work as a GPIO for output to HIGH. that will steer EIM_D18 to I2C3_SDA

Thanks

seungik Lee

0 件の賞賛
返信
7,337件の閲覧回数
weidong_sun
NXP TechSupport
NXP TechSupport

Hello, Lee,

OK, Can you send your BSP file to me ? Let me see it !

My personal email: [email protected]


weidong

0 件の賞賛
返信
7,337件の閲覧回数
leeseungik
Contributor III

What file exactly? uboot source? or kernel?

0 件の賞賛
返信
7,337件の閲覧回数
weidong_sun
NXP TechSupport
NXP TechSupport

Linux bsp file for your own board , like : board-mx6q_sabresd.c and it's .h file.

weidong

0 件の賞賛
返信
7,337件の閲覧回数
weidong_sun
NXP TechSupport
NXP TechSupport

Hello,lee,

     try to adjust the following:

#define __SILEE_275_UART4__ 1
#define __SILEE_275_ENET__ 1
#define __SILEE_275_WEIM_NOR__ 0
#define __SILEE_275_OPTIMIZE__ 1
#define __SILEE_275_I2C3__ 1

#define MX6Q_SABRELITE_SD3_CD  IMX_GPIO_NR(7, 0)
#define MX6Q_SABRELITE_SD3_WP  IMX_GPIO_NR(7, 1)
#define MX6Q_SABRELITE_SD4_CD  IMX_GPIO_NR(2, 6)
#define MX6Q_SABRELITE_SD4_WP  IMX_GPIO_NR(2, 7)
#define MX6Q_SABRELITE_USB_OTG_PWR IMX_GPIO_NR(3, 22)
#define MX6Q_SABRELITE_USB_HUB_RESET IMX_GPIO_NR(7, 12)
#define MX6Q_SABRELITE_ECSPI1_CS1 IMX_GPIO_NR(3, 19)
#define MX6Q_SABRELITE_CAP_TCH_INT1 IMX_GPIO_NR(1, 9)
#define MX6Q_SABRELITE_CSI0_RST  IMX_GPIO_NR(1, 8)
#define MX6Q_SABRELITE_CSI0_PWN  IMX_GPIO_NR(1, 6)
#define MX6Q_SABRELITE_CAN1_STBY IMX_GPIO_NR(1, 2)
#define MX6Q_SABRELITE_CAN1_EN  IMX_GPIO_NR(1, 4)
//#if __SILEE_275_WEIM_NOR__
#define SABREAUTO_WEIM_NOR_WDOG1    IMX_GPIO_NR(4, 29)
#define SABREAUTO_I2C3_STEER        IMX_GPIO_NR(5, 4)
//#endif

/*#if __SILEE_275_I2C3__

#define SABREAUTO_I2C3_STEER        IMX_GPIO_NR(5, 4)

#endif*/

      I can't confirm the issue is here, but let us try .

Weidong

0 件の賞賛
返信
7,338件の閲覧回数
leeseungik
Contributor III

It’s working now the problem is I set gpio output so early before gpio chip not initialized.

I move gpio_request and output to end of board_init then It works.

Your reply is really helpful to solve it. Thanks.

BR

  Seungik Lee

0 件の賞賛
返信