fsl-arm-yocto-bsp-imx-4.1-krogoth

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

fsl-arm-yocto-bsp-imx-4.1-krogoth

1,740 次查看
末班车上的乘客
Contributor II

repo init -u git://git.freescale.com/imx/fsl-arm-yocto-bsp.git -b imx-4.1-krogoth -m imx-4.1.15-2.1.0.xml
fatal: Cannot get https://gerrit.googlesource.com/git-repo/clone.bundle
fatal: error [Errno -3] Temporary failure in name resolution

from china

标签 (2)
0 项奖励
回复
1 回复

1,262 次查看
gusarambula
NXP TechSupport
NXP TechSupport

Hello  贾继中 贾继中 ,

I would recommend checking that you have the repo utility installed. You can install it with the commands on the following link:

FSL Community BSP 

I would also recommend making sure that you have internet access. It's common to have problems when under a firewall or trough a proxy so please review that you can reach git repositories.

I hope this helps!

Regards,

0 项奖励
回复