I.mx pins tool missing packege

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

I.mx pins tool missing packege

627 Views
yanivbeniluz
Contributor I

Hello,

I can not find the MCIMX6Y2DVK09AB in LFBGA272 i can only select the following:

processor: MCIMX6Y2xxx09
package_id: MCIMX6Y2DVM09

the DVK variant is the smaller package but is not showing even when i try to change the package

i am using V4.1

Labels (1)
0 Kudos
Reply
1 Reply

528 Views
gusarambula
NXP TechSupport
NXP TechSupport

Hello Yaniv Beniluz,

There are some packaging options missing for the i.MX6ULL on the latest version of the Pins Tool. Thanks for pointing this omission out, we have escalated this so the missing package configuration gets added.

The only available alternative in the LFBGA272 package is MCIMX6Y7xxx05 which you should be able to use as reference for your design in the meantime. Are you being able to see this alternative on the Pins Tool? If no more alternatives are showing it could be that the NXP repository cannot be reached, as the Pins Tool fetches the available configurations from the web.

I hope this helps!

Regards,

0 Kudos
Reply