frame rate issue

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

frame rate issue

803件の閲覧回数
muralikrishnant
Contributor I

Hai;

currently i am working under imx6 processor with parallel camera module ,i done the camera interface and live streaming also,but only we got 15 fps as per my requirement i need achive minimum of 30 fps ,so kindly provided any solution to over come this problem and i tried using mxc out but its give QBUF and DQBUF .

i am using YUYV format to capture camera data and i converted to RGB24 using image converter ic  and i directly write into frame buffer fbo

0 件の賞賛
返信
1 返信

749件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Muralikrishnan

performance may be affected by IC conversion times, so to narrow down issue one

can try to remove conversion routines or try with baremetal SDK IPU camera tests

Github SDK
https://github.com/backenklee/swp-report/tree/master/iMX6_Platform_SDK

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!

0 件の賞賛
返信