flexspi xip mode boot

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

flexspi xip mode boot

1,524件の閲覧回数
双朋赵
Contributor III

hello,everyone

as we know, there is one cortex-M4F core in i.MX8QXP MEK, we try to use this mcu other than extenal mcu, such as s32k, but the imaged released by nxp in L4.14.98_2.0.0_ga_images_MX8QXPMEK does not include any xip boot file, do you have plan to release the new image including the image using flexspi xip image to boot. 

ラベル(1)
0 件の賞賛
返信
1 返信

1,454件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi zhao

I am afraid except existing no more additional images are planned.

If you need some special image suggest to discuss that in local nxp marketing office.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信