flashing redboot on mx27ads board

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

flashing redboot on mx27ads board

2,892件の閲覧回数
ronj
Contributor I
hi,
 
i have an imx27ads board which was working fine - redboot+linux.
after erasing the flash, i;m trying to reprogram redboot with the pre-built binary.
i get the following output on the uart, after which it hangs.
 
++... Read from 0x07ee0000-0x07f00000 at 0xc1fe0000: .
... Read from 0x07ed3000-0x07ed4000 at 0xc1fff000: .
Ethernet FEC MAC address: is not set
Board Type: ADS
Clock input: 32KHz
Booting from [SDRAM]
FEC not connect right PHY: ID=fc1ffc
 
 
any ideas, suggestions ?
0 件の賞賛
返信
1 返信

1,663件の閲覧回数
rogerio_silva
NXP Employee
NXP Employee
Hi ronj,

   Check if you are programming the right binary that came with your ltib package (It's important considering that has many .bin versions).
 
   Are you adding a script to start redboot? Are you trying to boot with NFS or JFFS2 file system?

   Regards,

Rogerio.
0 件の賞賛
返信