flashcp MTD flash device failed

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

flashcp MTD flash device failed

Jump to solution
6,068 Views
davidzhou
Contributor V

Hi,

I have imx6ul dev board.

I use flashcp to update data file in the mtd flash device. The mtd partition is created through uboot as ubi format. The flashcp doesn't return any errors. After copy, the flash partition causes the problem.

At uboot, the command :

ubi part nand0,6

returns error:

ubi int err 22

which is working before flashcp command

The kernel uses

    .compatible = "fsl,imx6ul-gpmi-nand", device driver  (gpmi-nand.c)

the gpmi_nand_id_table[] includes imx6ul-gpmi-nand.

What else needs to be set or corrected?

  Thank You,

David Zhou

0 Kudos
Reply
1 Solution
5,290 Views
igorpadykov
NXP Employee
NXP Employee

Hi David

one can try with latest L4.9.11 nxp official kernel described on

i.MX Software|NXP 

and post issue on kernel mail list, note nxp uses only mfg tools as standard

way for updating images.

Majordomo Lists at VGER.KERNEL.ORG 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
2 Replies
5,291 Views
igorpadykov
NXP Employee
NXP Employee

Hi David

one can try with latest L4.9.11 nxp official kernel described on

i.MX Software|NXP 

and post issue on kernel mail list, note nxp uses only mfg tools as standard

way for updating images.

Majordomo Lists at VGER.KERNEL.ORG 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply
5,287 Views
davidzhou
Contributor V

Igor,

Thank you,

David Zhou

0 Kudos
Reply