I use i.MX8MQ.
I want to flash u-boot to emmc by using uboot.
I run the follow commands:
fatload mmc 0:1 ${loadaddr} flash.bin
mmc write ${loadaddr} 0x21 <u-boot image size in blocks>but, failed. I also try change 0x21 to 0x42 or 0x2 ,all fails.
Please help me,thank you very much!
解決済! 解決策の投稿を見る。
Hi 1053387324
for various emmc programming options one can look at
https://boundarydevices.com/programming-emmc-on-i-mx-platforms/
Best regards
igor
I also try the u-boot ums function.
when in host ubuntu, I find the new device /dev/sdb , /dev/sdb1, /dev/sdb2,then I use the fllow command to flash img
sudo dd if=$BOOT_DIR/flash.bin of=/dev/sdb seek=33 bs=1k conv=fsync
the u-boot version is not changed.
Hi 1053387324
for various emmc programming options one can look at
https://boundarydevices.com/programming-emmc-on-i-mx-platforms/
Best regards
igor