eMMC having TLC NAND Flash

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

eMMC having TLC NAND Flash

3,194件の閲覧回数
vinoth_ta
Contributor I

Hello,

It is noted that IMX8M will support MLC,SLC and Toggle NAND flash. Also support eMMC  version upto 5.1 (if use latest bsp). I could see high density eMMC5.1 may have TLC NAND Flash in it .

Shall we still use the eMMC having TLC type of NAND Flash in it?

I got below response from NXP support  " as I known, imx8M can support emmc 5.1" :smileyhappy:

Thanks you!

Regards,

Vinoth TA

ラベル(1)
タグ(1)
0 件の賞賛
返信
3 返答(返信)

3,064件の閲覧回数
Yuri
NXP Employee
NXP Employee

Hello,

  IMX8M documentation (Reference Manual, DataSheets) state, that eMMC 5.0 is supported.

This means, that devices of eMMC 5.1 can be used as much as they are backward compatible

with eMMC 5.0.


Have a great day,
Yuri.

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 件の賞賛
返信

3,064件の閲覧回数
vinoth_ta
Contributor I

Hi Yur,

Thanks. Shall we still use the eMMC having TLC type of NAND Flash in it?

Regards,

Vinoth TA

0 件の賞賛
返信

3,064件の閲覧回数
Yuri
NXP Employee
NXP Employee

Hello,

   As I understand - specifics of NAND, used in eMMC devices, is internal eMMC issue, 

and this does not affect eMMC (external) interface. So, customers can use i.MX8M with

any eMMC, satisfying the 5.0 specs.   

Regards,

Yuri.

0 件の賞賛
返信