eMMC booting error

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

eMMC booting error

1,568 次查看
mohammedazlum
Contributor IV

Hello,

I am using iMX6S procesor in our board. We could program Eboot+NK.bin into the eMMC. But couldn't boot the board from eMMC. I am getting below error when I compared the logs with working board while programming.

Could you suggest the solution ?

Old situation:

Warning: The partition table looks like it was made

for C/H/S=*/1/0 (instead of 461824/1/16).

For this listing I'll assume that geometry.

Regards,

Azlum

2 回复数

1,463 次查看
SergioSolis
NXP Employee
NXP Employee

hello Mohammed,

Are you trying to install a windows release?, did you download it from a third party company?

1,463 次查看
mohammedazlum
Contributor IV

Hi Serch,

We are trying to program WEC7 [also tied with Linux BSP]. But the result is any BSP [Linux/Android/Linux] not able to boot from eMMC.

Note that, I could boot the same board from SD card. After booting I could access the user area of eMMC, which means I could copy and paste contents to and from eMMC.

Regards,

Azlum

0 项奖励
回复