eMMC Initialization Progress in i.MX6S ROM

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

eMMC Initialization Progress in i.MX6S ROM

1,464件の閲覧回数
erickang
Contributor II

Hi All,

I have a problem to boot with eMMC in i.MX6S.

So I want to know how to initialize the eMMC in i.MX6S ROM.

I'm using the i.MX6S revision 1.2 and revision 1.3.

Actually I could know the eMMC initialization progress in u-boot based on <u-boot>/driver/mmc/mmc.c

But It was difficult to analyze the eMMC Initialization progress in i.MX6S ROM.

Could you tell me the eMMC Initialization progress in i.MX6S ROM revision 1.2 and revision 1.3?

Actually I want to know the eMMC Command and Response during the eMMC Initialization in i.MX6S ROM.

Best Regards,

Eric.


ラベル(2)
タグ(4)
0 件の賞賛
返信
1 返信

694件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Eric

for eMMC Initialization progress please look at

Figure 8-10. Expansion Device Boot Flow (1 of 6) IMX6SDLRM

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信