Detail of i.MX6SDL HDMI regsiters.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Detail of i.MX6SDL HDMI regsiters.

Jump to solution
579 Views
satoshishimoda
Senior Contributor I

Hi community,

We have a question about i.MX6SDL HDMI.

Please see chapter 34.5.314 ~ 34.5.321 in IMX6SDLRM (Rev.1).

There are no descriptions for these registers.

Would you let me know the detail of these registers?

Best Regards,

Satoshi Shimoda

Labels (2)
Tags (1)
0 Kudos
1 Solution
451 Views
Yuri
NXP Employee
NXP Employee

The following *CNT registers must be set before any I2C bus transaction
can take place to ensure proper I/O timing. The *CNT registers are:

-       *_I2CM_SS_SCL_HCNT

-       *_I2CM_SS_SCL_LCNT

-       *_I2CM_FS_SCL_HCNT

-       *_I2CM_FS_SCL_LCNT

The following abbreviation is used for I2C SCL clock settings:

•       SS: Standard Speed

•       FS: Fast Speed

•       HCNT: SCL High Level counter

•       LCNT: SCL Low Level counter


Have a great day,
Yuri.
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
452 Views
Yuri
NXP Employee
NXP Employee

The following *CNT registers must be set before any I2C bus transaction
can take place to ensure proper I/O timing. The *CNT registers are:

-       *_I2CM_SS_SCL_HCNT

-       *_I2CM_SS_SCL_LCNT

-       *_I2CM_FS_SCL_HCNT

-       *_I2CM_FS_SCL_LCNT

The following abbreviation is used for I2C SCL clock settings:

•       SS: Standard Speed

•       FS: Fast Speed

•       HCNT: SCL High Level counter

•       LCNT: SCL Low Level counter


Have a great day,
Yuri.

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos