eMMC Initialization Progress in i.MX6S ROM

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

eMMC Initialization Progress in i.MX6S ROM

1,443 次查看
erickang
Contributor II

Hi All,

I have a problem to boot with eMMC in i.MX6S.

So I want to know how to initialize the eMMC in i.MX6S ROM.

I'm using the i.MX6S revision 1.2 and revision 1.3.

Actually I could know the eMMC initialization progress in u-boot based on <u-boot>/driver/mmc/mmc.c

But It was difficult to analyze the eMMC Initialization progress in i.MX6S ROM.

Could you tell me the eMMC Initialization progress in i.MX6S ROM revision 1.2 and revision 1.3?

Actually I want to know the eMMC Command and Response during the eMMC Initialization in i.MX6S ROM.

Best Regards,

Eric.


标签 (2)
标记 (4)
0 项奖励
回复
1 回复

673 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Eric

for eMMC Initialization progress please look at

Figure 8-10. Expansion Device Boot Flow (1 of 6) IMX6SDLRM

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复