eIQ based sample application-Tflite face recognition CPP app stuck with compilation errors

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

eIQ based sample application-Tflite face recognition CPP app stuck with compilation errors

1,436 Views
rmani0029
Contributor I

I am facing the following compilation errors while trying to compile the eiq tflite based face_recognition sample application through the latest built fsl-imx-wayland-glibc-x86_64-imx-image-full-aarch64-toolchain-5.4-zeus SDK.

Error logs :

---------------------------

imx8@imx8:~/eIQ_NXP/eiq_sample_apps/examples-tflite/face_recognition/src$ make -f Makefile.linux
aarch64-poky-linux-g++ --sysroot=/opt/fsl-imx-wayland/5.4-zeus-new/sysroots/aarch64-poky-linux -o FaceRecognition -I /opt/fsl-imx-wayland/5.4-zeus-new/sysroots/aarch64-poky-linux/usr/include/tensorflow/lite/tools/make/downloads/flatbuffers/include/ face_recognition.cpp face_detect_helpers.cpp -ltensorflow-lite -lpthread -lrt -ldl -g -lopencv_objdetect -lopencv_highgui -lopencv_imgproc -lopencv_core -lopencv_videoio -lopencv_imgcodecs
/opt/fsl-imx-wayland/5.4-zeus-new/sysroots/x86_64-pokysdk-linux/usr/libexec/aarch64-poky-linux/gcc/aarch64-poky-linux/9.2.0/real-ld: cannot find -ltensorflow-lite
collect2: error: ld returned 1 exit status
Makefile.linux:13: recipe for target 'FaceRecognition' failed
make: *** [FaceRecognition] Error 1

So, Kindly help me on how to solve those compilation errors.

Regards,

Manikandan.R

0 Kudos
Reply
1 Reply

1,420 Views
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello mani0029,

Generally this problem occurred when we have called a function which has not been define in the program file, so to sort out this problem check whether have you called such function which has not been define in the program file. or you miss to install some package.

 

Regards

 

0 Kudos
Reply