directfb examples showing up weird on HDMI

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

directfb examples showing up weird on HDMI

ソリューションへジャンプ
1,954件の閲覧回数
rebelalliance
Contributor III

Hi,

Using SabreSD with i.MX6Q and Linux 4.0.0 SDK.

I compiled directfb-1.4.0 and directfb-examples that are included in the SDK.  I run the examples and they are coming out all screwed up on my HDMI monitor.  I am attaching screenshots of how they are on my system and how they are supposed to look.  It looks like the graqphics are displayed 4 times in 4 quadrants of the screen and the color is messed up.  What can be causing this?

df_andi expected:

directfb-examples-df-andi.jpg

df_andi observed:

IMG-20130628-00112.jpg

df_neo expected:

directfb-examples-df-neo.jpg

df_neo observed:

IMG-20130628-00111.jpg

ラベル(3)
タグ(2)
0 件の賞賛
返信
1 解決策
1,165件の閲覧回数
isaac_ng
NXP Employee
NXP Employee

Please try to rename or remove the file /etc/fb.modes  If you run the /usr/bin/df_andi and take a look on the console printout, it is set to 640x480 according to the /etc/fb.modes first setting. These are results of running /usr/bin/df_andi and /usr/bin/df_neo

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,166件の閲覧回数
isaac_ng
NXP Employee
NXP Employee

Please try to rename or remove the file /etc/fb.modes  If you run the /usr/bin/df_andi and take a look on the console printout, it is set to 640x480 according to the /etc/fb.modes first setting. These are results of running /usr/bin/df_andi and /usr/bin/df_neo

0 件の賞賛
返信