dhcp

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

dhcp

1,877件の閲覧回数
niklasmolin
Senior Contributor I

Hi.

I'm trying to configure dhcp on i.MX6 (built in Yocto).

It seems like if I have interface set to DHCP and there is no network connection, it tries a few times, but then stops.

Is there a way to configure this to continue to try or to have a fallback static address, like there is in Ubuntu (dhclient.conf using static leases if there is a timeout)?

Thanks,

Niklas

ラベル(2)
0 件の賞賛
返信
1 返信

1,595件の閲覧回数
jamesbone
NXP TechSupport
NXP TechSupport

Hello Niklas,

Can you please describe the network scenario where you are trying to connect the board?, Are you using a Router or Switch to provide the IP address or it is a server? do you have any segmentation  or any other filter that not allow to have the DHCP request that not came into the network?.  Do you set the MAC Address of the boarD?  If you set the IP static address always works?.

The BSP does not have something like the dhclient.conf, but it can be done usign the same packages that contains ubuntu. But this need to be done at Uboot.


Have a great day,
Jaime

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信