devregs problems ... Error reading CPU type

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

devregs problems ... Error reading CPU type

1,722 Views
fabio_poiatti
Contributor III

I have a IMX6ULLEVK board with installed devregs

Calling devregs I see:

Error reading CPU type

This is my /proc/cpuinfo

processor : 0
model name : ARMv7 Processor rev 5 (v7l)
BogoMIPS : 3.00
Features : half thumb fastmult vfp edsp neon vfpv3 tls vfpv4 idiva idivt vfpd32 lpae
CPU implementer : 0x41
CPU architecture: 7
CPU variant : 0x0
CPU part : 0xc07
CPU revision : 5

Hardware : Freescale i.MX6 UltraLite (Device Tree)
Revision : 0000
Serial : 0000000000000000

0 Kudos
Reply
2 Replies

1,610 Views
igorpadykov
NXP Employee
NXP Employee

Hi Fabio

seems there is no  .dat files for that processor, one can check answer on

similar issue on

devregs support for 6sololite 

imx-utils/devregs.cpp at master · boundarydevices/imx-utils · GitHub 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

1,610 Views
fabio_poiatti
Contributor III

Error CPU type seem to be related to Revision equal 0 ...and -c option to set from the shell the cpu name is not working

giving the error 

"unknown option c"

In addiction, the file /proc/cpuinfo I'm not able to modify setting a different revision

thanks

0 Kudos
Reply