devmem2 giving bus error on imx8mq linux

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

devmem2 giving bus error on imx8mq linux

1,912 Views
mahesh_hns
Contributor II

Hello,

 I was trying to read the SW_MUX_CTL_PAD_SD1_DATA4 SW MUX Control register (0x3033_00B8) using devmem2 on imx8mQ processor running linux (5.15) and got this

devmem2 0x303300B8
/dev/mem opened.
Memory mapped at address 0xffff9abd1000.
Bus error

I never had any issues like these while reading the mux registers on imx8mP processor. 
Why is that? What do I  need to do to read the pad/mux registers on imx8mQ ?

Thanks in advance

0 Kudos
Reply
1 Reply

1,878 Views
Zhiming_Liu
NXP TechSupport
NXP TechSupport

Hi

 

 

We can read this register on EVK board. 

root@imx8mqevk:/unit_tests# ./memtool -32 0x303300B8 1
E
Reading 0x1 count starting at address 0x303300B8

0x303300B8:  00000000



Best Regards
Zhiming

0 Kudos
Reply