I see the guide asks for an ATF compilation with the argument SPD=opteed.
Whenever I compile with this argument the ATF gets stuck after printing BL31: Initializing BL32. Specifically after the call to opteed_enter_sp().
Does the device need to be closed for this to work?
Maybe there is something wrong with my compilation of OP-TEE?
Can you tell me which specific values would I need for these OPTEE variables to make it run on the Pollux board? I've tried with the default values for the mx8mpevk flavor but they don't seem ok to me. So i've also tried with these:
- CFG_DDR_SIZE = UL(0x80000000)
- CFG_UART_BASE = UART1_BASE
- CFG_TZDRAM_SIZE = 0x01e00000
- CFG_TZDRAM_START = 0x56000000
- CFG_SHMEM_SIZE = 0x00200000
- CFG_SHMEM_START = 0x57e00000
For the u-boot I'm going with the "phycore-imx8mp" defconfig. Do I have to change something in the device tree? The one that the target is using is "imx8mp-phyboard-pollux-rdk"