decrease imx8mq cpu clk rate and gpu clk rate

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

decrease imx8mq cpu clk rate and gpu clk rate

2,363件の閲覧回数
nccpu
Contributor I

Hi,

I want to decrease imx8mq cpu clk from 800MHz-1300MHz to 500MHz-600MHz and gpu clk from 800MHz to 500MHz. How can I do? I use imx8mq evk board and BSP android9.0.2.

Thanks!

タグ(1)
0 件の賞賛
返信
3 返答(返信)

2,356件の閲覧回数
nccpu
Contributor I

@nxp TechSupport ,can you give me some suggestions?

0 件の賞賛
返信

2,345件の閲覧回数
BiyongSUN
NXP Employee
NXP Employee

For the cpu, you can use the DVFS CPU governor. 

It is pure linux knowledge, not for this i.MX Processor. it is the same linux knowledge for X86/X64. 

 

For the gpu, please read the BSP release document to use 

GPU DFS

 

Untitled.png

0 件の賞賛
返信

2,339件の閲覧回数
BiyongSUN
NXP Employee
NXP Employee

gpu: gpu@38000000 {
compatible = "vivante,gc";
reg = <0x38000000 0x40000>;
interrupts = <GIC_SPI 3 IRQ_TYPE_LEVEL_HIGH>;
clocks = <&clk IMX8MQ_CLK_GPU_ROOT>,
<&clk IMX8MQ_CLK_GPU_SHADER_DIV>,
<&clk IMX8MQ_CLK_GPU_AXI>,
<&clk IMX8MQ_CLK_GPU_AHB>;
clock-names = "core", "shader", "bus", "reg";
#cooling-cells = <2>;
assigned-clocks = <&clk IMX8MQ_CLK_GPU_CORE_SRC>,
<&clk IMX8MQ_CLK_GPU_SHADER_SRC>,
<&clk IMX8MQ_CLK_GPU_AXI>,
<&clk IMX8MQ_CLK_GPU_AHB>,
<&clk IMX8MQ_GPU_PLL_BYPASS>;
assigned-clock-parents = <&clk IMX8MQ_GPU_PLL_OUT>,
<&clk IMX8MQ_GPU_PLL_OUT>,
<&clk IMX8MQ_GPU_PLL_OUT>,
<&clk IMX8MQ_GPU_PLL_OUT>,
<&clk IMX8MQ_GPU_PLL>;
assigned-clock-rates = <800000000>, <800000000>,
<800000000>, <800000000>, <0>;
power-domains = <&pgc_gpu>;
status = "disabled";

0 件の賞賛
返信