debian-armhf port started!

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

debian-armhf port started!

2,534件の閲覧回数
KonstantinosMar
Contributor I
Mentioned also on: http://www.powerdeveloper.org/forums/viewtopic.php?p=13645#13645

Basically, the new port is built with -mfloat-abi=hard, and tuned for armv7-a cpus. Should offer substantially better performance than both Debian's armel port but also than Ubuntu's armel port (as this one is softfp only). We're moving quite fast and are up to 100 packages already -the fact that we already have a hardfp karmic port helps greatly!
タグ(1)
0 件の賞賛
返信
3 返答(返信)

2,262件の閲覧回数
KrishnaPavan
Contributor II

Can You Please explain the basic advantage of using armhf apart from that mentioned in here at the link http://wiki.debian.org/ArmHardFloatPort.

Is it just a usual Debian Kernel or what else?

Regards :: Krishna Pavan

0 件の賞賛
返信

2,262件の閲覧回数
zhiyancao
Contributor II

freescale i.mx515 evk is now only privide toolchain towards softfp, and when toolchain towards hard is ready?

Another, freescale provide amd-gpu-armel.deb, when provide *-armhf.deb?

0 件の賞賛
返信

2,262件の閲覧回数
KonstantinosMar
Contributor I
All info posted to debian-arm list: http://lists.debian.org/debian-arm/2010/08/msg00008.html For the impatient, here is the repo: deb http://freevec.org/repository main and a small tarball (no gui, no kernel/modules yet)http://freevec.org/repository/images/armhf-unstable-main.tar.lzmamd5sum: 6c473e570daccd5f622c95419fe2aa62 More packages are being added all the time and soon we'll have the first debian-armhf autobuilder! Stay tuned!
0 件の賞賛
返信