custom image sensor driver

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

custom image sensor driver

9,558件の閲覧回数
zohargolan
Contributor II

Hello NXP community,

I am trying to write a driver for our custom MIPI camera for IMX8MP device. The camera is acting as the master on the MIPI bus, and is generating the MIPI clock by itself. I am using Yocto Mickledore. I could not find anywhere information if this mode of operation is supported. I did see that all the drivers I was looking at have the clock generated as part of the driver. Is this mode supported and what do I need to do in the driver to disable the host MIPI clock and only use the sensor clock

Any suggestion will be appreciated

Thank you,

Zohar

0 件の賞賛
返信
7 返答(返信)

9,527件の閲覧回数
jimmychan
NXP TechSupport
NXP TechSupport

Could you show me how you connect the camera to i.MX8MP?

0 件の賞賛
返信

9,491件の閲覧回数
zohargolan
Contributor II

Hi Jimmy,

I connected the camera on the MIPI bus using 4 lanes with a clock of 504MHz.

I also connected GPIOs and I2C, but the camera at this moment does not use any of those signals and start streaming MIPI data on power on

0 件の賞賛
返信

9,443件の閲覧回数
jimmychan
NXP TechSupport
NXP TechSupport

What is the camera?

Do you mean the camera driver cannot control the camera? Is there any error message when you use the camera to capture?

0 件の賞賛
返信

9,432件の閲覧回数
zohargolan
Contributor II

Hi Jimmy,

Thank you for coming back to me. Here is what I have. I am working on a custom driver for my MIPI CSI2 camera. The camera (at current configuration) does not have any power control, reset control, and I2C control. It just start sending data on the 4 lanes MIPI port at power on.

This is the strip down simplistic driver I am trying

#include <asm/unaligned.h>
#include <linux/acpi.h>
#include <linux/delay.h>
#include <linux/i2c.h>
#include <linux/module.h>
#include <media/v4l2-ctrls.h>
#include <media/v4l2-device.h>
#include <media/v4l2-fwnode.h>
 
#define xxxxxx_LINK_FREQ 504000000ULL
 
#define xxxxxx_VIDEO_WIDTH 1280
#define xxxxxx_VIDEO_HEIGHT 960
 
#define xxxxxx_DATA_LANES 4
#define xxxxxx_RGB_DEPTH 8
 
#define xxxxxx_CSI_PIXEL_RATE (xxxxxx_LINK_FREQ * 2 * xxxxxx_DATA_LANES / \
xxxxxx_RGB_DEPTH)
 
#define xxxxxx_FLL_90FPS 0x0500
#define xxxxxx_FLL_90FPS_MIN 0x0500
#define xxxxxx_FLL_MAX 0x7fff
 
/* Exposure controls from sensor */
#define xxxxxx_REG_EXPOSURE 0x0074
#define xxxxxx_EXPOSURE_MIN 6
#define xxxxxx_EXPOSURE_MAX_MARGIN 2
#define xxxxxx_EXPOSURE_STEP 1
 
/* Analog gain controls from sensor */
#define xxxxxx_REG_ANALOG_GAIN 0x0077
#define xxxxxx_ANAL_GAIN_MIN 0
#define xxxxxx_ANAL_GAIN_MAX 240
#define xxxxxx_ANAL_GAIN_STEP 1
 
/* Digital gain controls from sensor */
#define xxxxxx_DGTL_GAIN_MIN 0
#define xxxxxx_DGTL_GAIN_MAX 2048
#define xxxxxx_DGTL_GAIN_STEP 1
#define xxxxxx_DGTL_GAIN_DEFAULT 256
 
enum {
xxxxxx_LINK_FREQ_INDEX,
};
 
struct xxxxxx_reg {
u16 address;
u16 val;
};
 
struct xxxxxx_reg_list {
u32 num_of_regs;
const struct xxxxxx_reg *regs;
};
 
struct xxxxxx_link_freq_config {
const struct xxxxxx_reg_list reg_list;
};
 
struct xxxxxx_mode {
/* Frame width in pixels */
u32 width;
 
/* Frame height in pixels */
u32 height;
 
/* Horizontal timining size */
u32 llp;
 
/* Default vertical timining size */
u32 fll_def;
 
/* Min vertical timining size */
u32 fll_min;
 
/* Link frequency needed for this resolution */
u32 link_freq_index;
 
/* Sensor register settings for this resolution */
const struct xxxxxx_reg_list reg_list;
};
 
#define to_xxxxxx(_sd) container_of(_sd, struct xxxxxx, sd)
 
static const char * const xxxxxx_test_pattern_menu[] = {
"Disabled",
"Solid Colour",
"100% Colour Bars",
"Fade To Grey Colour Bars",
"PN9",
"Gradient Horizontal",
"Gradient Vertical",
"Check Board",
"Slant Pattern",
};
 
static const s64 link_freq_menu_items[] = {
xxxxxx_LINK_FREQ,
};
 
static const struct xxxxxx_mode supported_modes[] = {
{
.width = xxxxxx_VIDEO_WIDTH,
.height = xxxxxx_VIDEO_HEIGHT,
.fll_def = xxxxxx_FLL_90FPS,
.fll_min = xxxxxx_FLL_90FPS_MIN,
.llp = 0x0b00,
.link_freq_index = xxxxxx_LINK_FREQ_INDEX,
}
 
};
 
struct xxxxxx {
struct v4l2_subdev sd;
struct media_pad pad;
struct v4l2_ctrl_handler ctrl_handler;
 
/* V4L2 Controls */
struct v4l2_ctrl *link_freq;
struct v4l2_ctrl *pixel_rate;
struct v4l2_ctrl *vblank;
struct v4l2_ctrl *hblank;
struct v4l2_ctrl *exposure;
 
/* Current mode */
const struct xxxxxx_mode *cur_mode;
 
/* To serialize asynchronus callbacks */
struct mutex mutex;
 
/* Streaming on/off */
bool streaming;
 
/* True if the device has been identified */
bool identified;
};
 
static int xxxxxx_s_power(struct v4l2_subdev *sd, int on)
{
struct xxxxxx *sensor = to_xxxxxx(sd);
int ret = 0;
 
mutex_lock(&sensor->mutex);
 
mutex_unlock(&sensor->mutex);
return ret;
}
 
 
 
static int xxxxxx_set_ctrl(struct v4l2_ctrl *ctrl)
{
struct xxxxxx *xxxxxx = container_of(ctrl->handler,
     struct xxxxxx, ctrl_handler);
struct i2c_client *client = v4l2_get_subdevdata(&xxxxxx->sd);
s64 exposure_max;
int ret = 0;
 
/* Propagate change of current control to all related controls */
if (ctrl->id == V4L2_CID_VBLANK) {
/* Update max exposure while meeting expected vblanking */
exposure_max = xxxxxx->cur_mode->height + ctrl->val -
       xxxxxx_EXPOSURE_MAX_MARGIN;
__v4l2_ctrl_modify_range(xxxxxx->exposure,
xxxxxx->exposure->minimum,
exposure_max, xxxxxx->exposure->step,
exposure_max);
}
 
switch (ctrl->id) {
case V4L2_CID_ANALOGUE_GAIN:
break;
 
case V4L2_CID_DIGITAL_GAIN:
break;
 
case V4L2_CID_EXPOSURE:
break;
 
case V4L2_CID_VBLANK:
/* Update FLL that meets expected vertical blanking */
break;
 
case V4L2_CID_TEST_PATTERN:
break;
 
default:
ret = -EINVAL;
break;
}
 
return ret;
}
 
static const struct v4l2_ctrl_ops xxxxxx_ctrl_ops = {
.s_ctrl = xxxxxx_set_ctrl,
};
 
static int xxxxxx_init_controls(struct xxxxxx *xxxxxx)
{
struct v4l2_ctrl_handler *ctrl_hdlr;
s64 exposure_max, h_blank;
int ret;
 
ctrl_hdlr = &xxxxxx->ctrl_handler;
ret = v4l2_ctrl_handler_init(ctrl_hdlr, 4);
if (ret)
return ret;
 
ctrl_hdlr->lock = &xxxxxx->mutex;
xxxxxx->link_freq = v4l2_ctrl_new_int_menu(ctrl_hdlr, &xxxxxx_ctrl_ops,
V4L2_CID_LINK_FREQ, ARRAY_SIZE(link_freq_menu_items) - 1, 0,
link_freq_menu_items);
if (xxxxxx->link_freq)
xxxxxx->link_freq->flags |= V4L2_CTRL_FLAG_READ_ONLY;
 
xxxxxx->pixel_rate = v4l2_ctrl_new_std
    (ctrl_hdlr, &xxxxxx_ctrl_ops,
     V4L2_CID_PIXEL_RATE, 0,
     xxxxxx_CSI_PIXEL_RATE,
     1,
xxxxxx_CSI_PIXEL_RATE);
xxxxxx->vblank = v4l2_ctrl_new_std(ctrl_hdlr, &xxxxxx_ctrl_ops,
  V4L2_CID_VBLANK,
  xxxxxx_FLL_90FPS_MIN -
  xxxxxx->cur_mode->height,
  xxxxxx_FLL_MAX -
  xxxxxx->cur_mode->height, 1,
  xxxxxx->cur_mode->fll_def -
  xxxxxx->cur_mode->height);
 
 
h_blank = xxxxxx->cur_mode->llp - xxxxxx->cur_mode->width;
xxxxxx->hblank = v4l2_ctrl_new_std(ctrl_hdlr, &xxxxxx_ctrl_ops,
  V4L2_CID_HBLANK, h_blank, h_blank, 1,
  h_blank);
if (xxxxxx->hblank)
xxxxxx->hblank->flags |= V4L2_CTRL_FLAG_READ_ONLY;
 
xxxxxx->sd.ctrl_handler = ctrl_hdlr;
 
return 0;
}
 
static void xxxxxx_assign_pad_format(const struct xxxxxx_mode *mode,
    struct v4l2_mbus_framefmt *fmt)
{
fmt->width = mode->width;
fmt->height = mode->height;
fmt->code = MEDIA_BUS_FMT_Y8_1X8;
fmt->field = V4L2_FIELD_NONE;
}
 
 
static int xxxxxx_set_stream(struct v4l2_subdev *sd, int enable)
{
/*
* Don't need to do anything here, just assume the source is streaming
* already.
*/
return 0;
}
 
static int xxxxxx_set_format(struct v4l2_subdev *sd,
    struct v4l2_subdev_state *sd_state,
    struct v4l2_subdev_format *fmt)
{
struct xxxxxx *xxxxxx = to_xxxxxx(sd);
const struct xxxxxx_mode *mode;
s32 vblank_def, h_blank;
 
mode = v4l2_find_nearest_size(supported_modes,
      ARRAY_SIZE(supported_modes), width,
      height, fmt->format.width,
      fmt->format.height);
 
mutex_lock(&xxxxxx->mutex);
xxxxxx_assign_pad_format(mode, &fmt->format);
if (fmt->which == V4L2_SUBDEV_FORMAT_TRY) {
*v4l2_subdev_get_try_format(sd, sd_state, fmt->pad) = fmt->format;
} else {
xxxxxx->cur_mode = mode;
__v4l2_ctrl_s_ctrl(xxxxxx->link_freq, mode->link_freq_index);
__v4l2_ctrl_s_ctrl_int64(xxxxxx->pixel_rate, xxxxxx_CSI_PIXEL_RATE);
 
/* Update limits and set FPS to default */
vblank_def = mode->fll_def - mode->height;
__v4l2_ctrl_modify_range(xxxxxx->vblank,
mode->fll_min - mode->height,
xxxxxx_FLL_MAX - mode->height, 1,
vblank_def);
__v4l2_ctrl_s_ctrl(xxxxxx->vblank, vblank_def);
 
h_blank = xxxxxx->cur_mode->llp - xxxxxx->cur_mode->width;
 
__v4l2_ctrl_modify_range(xxxxxx->hblank, h_blank, h_blank, 1,
h_blank);
}
 
mutex_unlock(&xxxxxx->mutex);
 
return 0;
}
 
static int xxxxxx_get_format(struct v4l2_subdev *sd,
    struct v4l2_subdev_state *sd_state,
    struct v4l2_subdev_format *fmt)
{
struct xxxxxx *xxxxxx = to_xxxxxx(sd);
 
mutex_lock(&xxxxxx->mutex);
if (fmt->which == V4L2_SUBDEV_FORMAT_TRY)
fmt->format = *v4l2_subdev_get_try_format(&xxxxxx->sd,
  sd_state,
  fmt->pad);
else
xxxxxx_assign_pad_format(xxxxxx->cur_mode, &fmt->format);
 
mutex_unlock(&xxxxxx->mutex);
 
return 0;
}
 
static int xxxxxx_enum_mbus_code(struct v4l2_subdev *sd,
struct v4l2_subdev_state *sd_state,
struct v4l2_subdev_mbus_code_enum *code)
{
if (code->index > 0)
return -EINVAL;
 
code->code = MEDIA_BUS_FMT_Y8_1X8;
 
return 0;
}
 
static int xxxxxx_enum_frame_size(struct v4l2_subdev *sd,
struct v4l2_subdev_state *sd_state,
struct v4l2_subdev_frame_size_enum *fse)
{
if (fse->index >= ARRAY_SIZE(supported_modes))
return -EINVAL;
 
if (fse->code != MEDIA_BUS_FMT_Y8_1X8)
return -EINVAL;
 
 
fse->min_width = supported_modes[fse->index].width;
fse->max_width = supported_modes[fse->index].width;
fse->min_height = supported_modes[fse->index].height;
fse->max_height = supported_modes[fse->index].height;
 
return 0;
}
 
static const struct v4l2_subdev_core_ops sensor_core_ops = {
.subscribe_event = v4l2_ctrl_subdev_subscribe_event,
.s_power = xxxxxx_s_power,
};
 
static int xxxxxx_open(struct v4l2_subdev *sd, struct v4l2_subdev_fh *fh)
{
struct xxxxxx *xxxxxx = to_xxxxxx(sd);
 
mutex_lock(&xxxxxx->mutex);
xxxxxx_assign_pad_format(&supported_modes[0],
v4l2_subdev_get_try_format(sd, fh->state, 0));
mutex_unlock(&xxxxxx->mutex);
 
return 0;
}
 
static const struct v4l2_subdev_video_ops xxxxxx_video_ops = {
.s_stream = xxxxxx_set_stream,
};
 
static const struct v4l2_subdev_pad_ops xxxxxx_pad_ops = {
.set_fmt = xxxxxx_set_format,
.get_fmt = xxxxxx_get_format,
.enum_mbus_code = xxxxxx_enum_mbus_code,
.enum_frame_size = xxxxxx_enum_frame_size,
};
 
static const struct v4l2_subdev_ops xxxxxx_subdev_ops = {
.video = &xxxxxx_video_ops,
.core = &sensor_core_ops,
.pad = &xxxxxx_pad_ops,
};
 
static int xxxxxx_link_setup(struct media_entity *entity,
   const struct media_pad *local,
   const struct media_pad *remote, u32 flags)
{
printk("xxxxxx - link setup");
return 0;
}
 
static const struct media_entity_operations xxxxxx_sd_entity_ops = {
.link_setup = xxxxxx_link_setup,
};
 
static const struct v4l2_subdev_internal_ops xxxxxx_internal_ops = {
.open = xxxxxx_open,
};
 
static void xxxxxx_remove(struct i2c_client *client)
{
struct v4l2_subdev *sd = i2c_get_clientdata(client);
struct xxxxxx *xxxxxx = to_xxxxxx(sd);
 
media_entity_cleanup(&sd->entity);
v4l2_ctrl_handler_free(sd->ctrl_handler);
mutex_destroy(&xxxxxx->mutex);
}
 
static int xxxxxx_probe(struct i2c_client *client)
{
struct xxxxxx *xxxxxx;
int ret;
 
xxxxxx = devm_kzalloc(&client->dev, sizeof(*xxxxxx), GFP_KERNEL);
printk("xxxxxx - kzalloc %d", xxxxxx);
if (!xxxxxx)
return -ENOMEM;
 
v4l2_i2c_subdev_init(&xxxxxx->sd, client, &xxxxxx_subdev_ops);
 
mutex_init(&xxxxxx->mutex);
xxxxxx->cur_mode = &supported_modes[0];
ret = xxxxxx_init_controls(xxxxxx);
printk("xxxxxx - xxxxxx_init_controls %d", ret);
if (ret) {
dev_err(&client->dev, "failed to init controls: %d", ret);
goto probe_error_v4l2_ctrl_handler_free;
}
 
xxxxxx->sd.internal_ops = &xxxxxx_internal_ops;
xxxxxx->sd.flags |= V4L2_SUBDEV_FL_HAS_DEVNODE;
xxxxxx->sd.entity.ops = &xxxxxx_sd_entity_ops;
xxxxxx->sd.entity.function = MEDIA_ENT_F_CAM_SENSOR;
xxxxxx->pad.flags = MEDIA_PAD_FL_SOURCE;
ret = media_entity_pads_init(&xxxxxx->sd.entity, 1, &xxxxxx->pad);
printk("xxxxxx - media_entity_pads_init %d", (int)ret);
if (ret) {
dev_err(&client->dev, "failed to init entity pads: %d", ret);
goto probe_error_v4l2_ctrl_handler_free;
}
 
ret = v4l2_async_register_subdev_sensor(&xxxxxx->sd);
printk("xxxxxx - v4l2_async_register_subdev_sensor %d", ret);
if (ret < 0) {
dev_err(&client->dev, "failed to register V4L2 subdev: %d",
ret);
goto probe_error_media_entity_cleanup;
}
 
printk("xxxxxx - finish probing");
return 0;
 
probe_error_media_entity_cleanup:
media_entity_cleanup(&xxxxxx->sd.entity);
 
probe_error_v4l2_ctrl_handler_free:
v4l2_ctrl_handler_free(xxxxxx->sd.ctrl_handler);
mutex_destroy(&xxxxxx->mutex);
 
return ret;
}
 
static const struct of_device_id xxxxxx_dt_ids[] = {
{ .compatible = "yyyyyy,xxxxxx" },
{},
};
MODULE_DEVICE_TABLE(of, xxxxxx_dt_ids);
 
static struct i2c_driver xxxxxx_i2c_driver = {
.driver = {
.name = "xxxxxx",
.of_match_table = xxxxxx_dt_ids,
},
.probe_new = xxxxxx_probe,
.remove = xxxxxx_remove,
};
 
module_i2c_driver(xxxxxx_i2c_driver);
 
MODULE_AUTHOR("Zohar Golan");
MODULE_DESCRIPTION("yyyyyy xxxxxx sensor driver");
MODULE_LICENSE("GPL v2");
 
at boot time, I can see in dmesg that the driver is loading with no errors (I have some printk that I removed from the code above).
 
I can see there are some new entries in v4l2-ctl

root@imx8mp-var-dart:~# v4l2-ctl --list-devices
[ 102.334469] mxc_isi.1: is_entity_link_setup, No remote pad found!
():
/dev/v4l-subdev0

FSL Capture Media Device (platform:32c00000.bus:camera):
/dev/media0

mxc-isi-cap (platform:32e00000.isi:cap_devic):
/dev/video3

mxc-isi-m2m (platform:32e00000.isi:m2m_devic):
/dev/video2

mxc-isi-cap (platform:32e02000.isi:cap_devic):
/dev/video4

vsi_v4l2dec (platform:vsi_v4l2dec):
/dev/video1

vsi_v4l2enc (platform:vsi_v4l2enc):
/dev/video0

 
however when I am checking the formats of the different drivers, I don't see what I am expecting

root@imx8mp-var-dart:~# v4l2-ctl -d /dev/video3 --list-formats
ioctl: VIDIOC_ENUM_FMT
Type: Video Capture Multiplanar

[0]: 'RGBP' (16-bit RGB 5-6-5)
[1]: 'RGB3' (24-bit RGB 8-8-8)
[2]: 'BGR3' (24-bit BGR 8-8-8)
[3]: 'YUYV' (YUYV 4:2:2)
[4]: 'YUV4' (32-bit A/XYUV 8-8-8-8)
[5]: 'NV12' (Y/UV 4:2:0)
[6]: 'NM12' (Y/UV 4:2:0 (N-C))
[7]: 'YM24' (Planar YUV 4:4:4 (N-C))
[8]: 'XR24' (32-bit BGRX 8-8-8-8)
[9]: 'AR24' (32-bit BGRA 8-8-8-8)

I expected to see GRAY8 or Y8
 
Also when I am trying the following gstreamer command
root@imx8mp-var-dart:~# gst-launch-1.0 v4l2src device=/dev/video3 ! waylandsink
[ 359.543456] mxc_isi.1: is_entity_link_setup, No remote pad found!
[ 359.948288] mxc_isi.1: is_entity_link_setup, No remote pad found!
Setting pipeline to PAUSED ...
Pipeline is live and does not need PREROLL ...
Pipeline is PREROLLED ...
Setting pipeline to PLAYING ...
New clock: GstSystemClock
[ 359.989811] isi-capture 32e00000.isi:cap_device: mxc_isi_source_fmt_init: src:(1280,960), dst:(3840,2160) Not support upscale
ERROR: from element /GstPipeline:pipeline0/GstV4l2Src:v4l2src0: Failed to allocate required memory.
Additional debug info:
/usr/src/debug/gstreamer1.0-plugins-good/1.22.0.imx-r0/sys/v4l2/gstv4l2src.c(977): gst_v4l2src_decide_allocation (): /GstPipeline:pipeline0/GstV4l2Src:v4l2src0:
Buffer pool activation failed
Execution ended after 0:00:00.027122983
Setting pipeline to NULL ...
ERROR: from element /GstPipeline:pipeline0/GstV4l2Src:v4l2src0: Internal data stream error.
Additional debug info:
/usr/src/debug/gstreamer1.0/1.22.0.imx-r0/libs/gst/base/gstbasesrc.c(3132): gst_base_src_loop (): /GstPipeline:pipeline0/GstV4l2Src:v4l2src0:
streaming stopped, reason not-negotiated (-4)
Freeing pipeline ...
 
 
Zohar

 

0 件の賞賛
返信

9,431件の閲覧回数
zohargolan
Contributor II

also if I am sending the following command GST_DEBUG=3 gst-launch-1.0 -v v4l2src device=/dev/video3 ! video/x-raw,width=1280,height=960,framerate=90/1 ! waylandsink

I don't get an error, and the GStreamer is not stopping, but no video is shown

root@imx8mp-var-dart:~# GST_DEBUG=3 gst-launch-1.0 -v v4l2src device=/dev/video3 ! video/x-raw,width=1280,height=960,framerate=90/1 ! waylandsink
Setting pipeline to PAUSED ...
Pipeline is live and does not need PREROLL ...
0:00:00.086316000 1809 0xaaaad3a1de40 WARN v4l2 gstv4l2object.c:4726:gst_v4l2_object_get_crop_rect:<v4l2src0:src> Failed to get default crop rectangle with VIDIOC_G_SELECTION: Invalid argument
0:00:00.086430500 1809 0xaaaad3a1de40 WARN v4l2 gstv4l2object.c:4927:gst_v4l2_object_probe_caps:<v4l2src0:src> Failed to probe pixel aspect ratio with VIDIOC_CROPCAP: Invalid argument
Pipeline is PREROLLED ...
Setting pipeline to PLAYING ...
New clock: GstSystemClock
/GstPipeline:pipeline0/GstV4l2Src:v4l2src0.GstPad:src: caps = video/x-raw, width=(int)1280, height=(int)960, framerate=(fraction)90/1, format=(string)YUY2, interlace-mode=(string)progressive, colorimetry=(string)1:4:5:1
/GstPipeline:pipeline0/GstCapsFilter:capsfilter0.GstPad:src: caps = video/x-raw, width=(int)1280, height=(int)960, framerate=(fraction)90/1, format=(string)YUY2, interlace-mode=(string)progressive, colorimetry=(string)1:4:5:1
/GstPipeline:pipeline0/GstWaylandSink:waylandsink0.GstPad:sink: caps = video/x-raw, width=(int)1280, height=(int)960, framerate=(fraction)90/1, format=(string)YUY2, interlace-mode=(string)progressive, colorimetry=(string)1:4:5:1
0:00:00.088664375 1809 0xaaaad3a1de40 WARN v4l2 gstv4l2object.c:4726:gst_v4l2_object_get_crop_rect:<v4l2src0:src> Failed to get default crop rectangle with VIDIOC_G_SELECTION: Invalid argument
/GstPipeline:pipeline0/GstCapsFilter:capsfilter0.GstPad:sink: caps = video/x-raw, width=(int)1280, height=(int)960, framerate=(fraction)90/1, format=(string)YUY2, interlace-mode=(string)progressive, colorimetry=(string)1:4:5:1
0:00:00.088779000 1809 0xaaaad3a1de40 WARN v4l2 gstv4l2object.c:3440:gst_v4l2_object_reset_compose_region:<v4l2src0:src> Failed to get default compose rectangle with VIDIOC_G_SELECTION: Invalid argument

0 件の賞賛
返信

9,144件の閲覧回数
Ohm86
Contributor I

Hello Zohargolan,

I am also writing adv7480 driverv for imx8MPlus with Mickledore . I am facing same issue "Failed to get default compose rectangle with VIDIOC_G_SELECTION: Invalid argument ".
I have tried same driver with imx8Mmini , its working fine.
But having issue with imx8Mplus. adv7480 is using external clock generator as clock source.

Have your issue resolved??
if yes then Can you please give me some inputs to resolve??
i have attached my log file. please look into this.

Thanks,


 

 

0 件の賞賛
返信

9,278件の閲覧回数
zohargolan
Contributor II

Hi @joanxie 

I know this is an old thread, but I have a similar problema and I cannot find a solution for it. I am trying to connect to a custom 8 bit grayscale sensor using V4l2, Currently I can get the gray image, using the ISI with code MEDIA_BUS_FMT_Y8_1X8 and the colorspace is V4L2_COLORSPACE_RAW, but the size is incorrect. I see 2 images side by side and the vertical size is also incorrect.

1. in your comment for the following post https://community.nxp.com/t5/i-MX-Processors/i-MX8-ISI-for-RAW8-and-RAW10-formats-grayscale-image-se... you mentioned to use the ISP instead of the ISI. Is there an example of how to do that?

2. Do you have other suggestions on how to implement the grayscale sensor?

 

Thank you,

Zohar

 

0 件の賞賛
返信