Hi
I received a couple of MX6 boards from the manufacturer EXCEET
they eventually sold part of the company, so there is no support of the boards anymore. I have no datasheet or such from these boards. There is a SD slot on the boards but it didnt come with any SD in it.
The only bit of info I have is the putty message that comes up when I connect my computer to one of the 2 USB ports of the board:
CPU: Freescale i.MX6SOLO rev1.1 at 792 MHz
CPU: Temperature 33 C, calibration data: 0x5cc52a69
Reset cause: WDOG
Board: MX6SEXCEET
DRAM: 512 MiB
force_idle_bus: sda=0 scl=1 sda.gp=0xcb scl.gp=0x5
NAND: 512 MiB
MMC: FSL_SDHC: 0
SF: Detected EN25Q80 with page size 64 KiB, total 1 MiB
*** Warning - bad CRC, using default environment
Net: FEC
Normal Boot
Hit any key to stop autoboot: 0
MMC: no card present
** Bad device mmc 0 **
MMC: no card present
** Bad device mmc 0 **
libfdt fdt_check_header(): FDT_ERR_BADMAGIC
Wrong Image Format for bootm command
ERROR: can't get kernel image!
U-Boot >
Can anyone help me how I could proceed from here?
thx
hey
unfortunately I coulndt find much useful for me on this pages...
I did write to the new owner Kontron but didnt get any answer yet...
I eventually received a board with a SD card, so I could get the files I needed. I have total 3 boards, 2 of them are now working with that SD card. One board though doesnt seem to do anything. 2 green LEDs light up as usual, the USB-serial port is recognized by my computer but there isnt any post. THis is the only one of the 3 boards where the second USB port is recognized as well, it shows up as "SE BLANK RIGEL"
can I do anything with that? can it be that uboot has been deleted from that board?