could maestro support recording audio from audio encode and save it to opus audio file

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

could maestro support recording audio from audio encode and save it to opus audio file

1,607 次查看
jichen0919_nxp
Contributor I

Greetings ,

I have one question regarding maestro audio framework,  there is one example that record audio from microphone and save it to pcm file, my question is does maestro framework support recording audio and save it to opus audio file,

can I implemented using a custom pipeline, including following 3 element,

TYPE_ELEMENT_AUDIO_SRC,TYPE_ELEMENT_ENCODER,ELEMENT_FILE_SINK_INDEX

thanks in advance.

0 项奖励
回复
2 回复数

1,554 次查看
jay_heng
NXP Employee
NXP Employee

We have below demo in SDK, it can record from MIC and save .pcm file into SD card (shellRecMIC), it can also encode a hardcoded pcm data buffer to opus format (shellOpusEncode), so we can refer to this demo and merge these two shellTasks

\SDK_2_14_0_MIMXRT1170-EVKB\boards\evkbmimxrt1170\audio_examples\maestro_record

0 项奖励
回复

1,566 次查看
brian14
NXP TechSupport
NXP TechSupport

Hi @jichen0919_nxp

Thank you for contacting NXP Support.

This software is unsupported for i.MX microprocessors family.
If you are using a microcontroller, please submit your question in the correct section.

Have a great day!

0 项奖励
回复