chromium hardware accelerate video decoding ,

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

chromium hardware accelerate video decoding ,

1,116件の閲覧回数
Asadeds
Contributor II

Hi NXP  Team ,


I am struggling to choice,  which  board is good for our project, which is based on high resolution playing video on the chromium . can anybody tell me.

0 件の賞賛
返信
1 返信

1,097件の閲覧回数
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello,

i.MX8 VPU hardware decoder support below video codec:

H.265 HEVC Main Profile 4Kp60 Level 5.1

H.264 AVC Constrained Baseline, Main and High profile

H.264 MVC

WMV9 / VC-1 Simple, Main and Advanced Profile

MPEG 1 and 2 Main Profile at High Level

AVS Jizhun Profile (JP)

MJPEG4.2 ASP, H.263, Sorenson Spark

Divx 3.11, with Global Motion Compensation (GMC)

ON2/Google VP6/VP8

RealVideo 8/9/10

JPEG and MJPEG A/B Baseline

 

i.MX8 VPU Linux driver is implemented based on V4L2 standard.

Chromium beside software video decoding, it also support hardware video decoder(VideoDecodeAccelerator), there are some kind of VideoDecodeAccelerator, one of them is V4L2VDA.

Please note V4L2VDA is using V4l2 api, so it is possible that change V4L2VDA to enable Chromium hardware video playback on i.MX8.

 

Regards

0 件の賞賛
返信