charging battery

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

charging battery

2,224 Views
idom
Contributor II

Hi

I use IMX8MMEVKHUG as a reference design.

Does the USB-OTG design support battery charging?

Is there any UG can guide me to connect 5.5-8V LI-PO to the design?

if I connect a battery to J101 will charge it  ?

Labels (1)
0 Kudos
Reply
2 Replies

2,100 Views
idom
Contributor II

I am looking for full datasheet of NX20P3483UK and PCA9468

Do you have any application note for PCA9468

0 Kudos
Reply

2,100 Views
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello Ido,

We don´t have a User Guide for the USB, but we have the general user guide you can downloaded from:

https://www.nxp.com/webapp/Download?colCode=IMX8MMEVKHUG 

https://www.nxp.com/webapp/Download?colCode=IMX8MMHDG 

On the board side There are two USB:

J301 is connected to the USB1 interface of the i.MX 8M Mini, which can act as the download port of the EVK.
J302 is connected to the USB2 interface of the i.MX 8M Mini, which can act as the power supply port of the EVK.

Regards

0 Kudos
Reply